Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description Go to description

Library Manager

The Library Manager window is accessed by selecting Waveform Library from the Tools Closeddrop-down menu. It enables you to import previously stored waveforms into the WaveformLibrary folder.

By using the Library Manager and its associated Import Waveform window, you can make adjustments to the Filter Ratio and have multiple Resample Targets... for each of your library waveforms, saving waveform generation time.

sd

 

File

Create Folder

Customize and organize your own waveform library folders. This function becomes active only when you click a folder in the Library Manager window.

Close

Exits the Library Manager.

Edit

Delete

Deletes a library waveform folder or library waveform.

Rename

Renames your library waveform folders and files.

Data

Resample

Adds additional sampling ratios to your library waveforms. This function becomes active only when you click on a library waveform.

Import Waveform

Opens the Import Waveform Closedwindow where you can import a previously stored waveform into the Library Manager. Click Source Waveform Name to select a waveform. This activates a wizard, which steps you through a few windows where you can make adjustments to the Filter Ratio and configure multiple Resample Targets for each of your library waveforms, saving time with your measurements. Signal Studio waveform files (*.wfm) and Matlab files (*.mat) are acceptable file formats. When using a Matlab file, you must manually set the Source Sampling Ratio. Convenient parameter descriptions and instructions appear at the bottom of each window the wizard steps you through.

Add to Signal Studio

Imports the currently selected library waveform into the Signal Studio's Waveform Setup node. This function becomes active only when you select a library waveform.

View

Refresh

Updates your view of the Waveform Library's folders and files.

Waveform Library

This area contains all your library waveform files. The parameters under Waveform Item Abstraction are not editable but provide information about the selected library waveform. Clicking any of these parameters displays a description below.

Library Waveform

Imported Waveform